Welcome to the Beta version of the Spirax Sarco website intended for final customer testing. During this beta phase, we will be fine tuning the website before the launch of the new website.

We use cookies to give you the best experience on our website. If you continue without changing your cookie settings, we assume that you consent to our use of cookies on this device. You can change your cookie settings at any time but if you do, you may lose some functionality on our website. More information can be found in our Privacy Policy.

Looking for Spirax Sarco products and services?

The Boiler House

Boiler ​R​atings 

This tutorial explains the three most commonly used boiler ratings: The 'From and at' rating for evaporation, the kW rating for heat output, and boiler horsepower.

'From and at' rating

The ‘from and at’ rating is widely used as a datum by shell boiler manufacturers to give a boiler a rating which shows the amount of steam in kg/h which the boiler can create ‘from and at 100°C’,at atmospheric pressure. Each kilogram of steam would then have received 2 257 kJ of heat from the boiler. 

Shell boilers are often operated with feedwater temperatures lower than 100°C. Consequently the boiler is required to supply enthalpy to bring the water up to boiling point.

Most boilers operate at pressures higher than atmospheric, because steam at an elevated pressure carries more heat energy than does steam at 100°C. This calls for additional enthalpy of saturation of water. As the boiler pressure rises, the saturation temperature is increased, needing even more enthalpy before the feedwater is brought up to boiling temperature.

Both these effects reduce the actual steam output of the boiler, for the same consumption of fuel.

The graph in Figure 3.5.1 shows feedwater temperatures plotted against the percentage of the ‘from and at’ figure for operation at pressures of 0, 5, 10 and 15 bar g.

The application of the ‘from and at’ rating graph (Figure 3.5.1) is shown in Example 3.5.1, as well as a demonstration of how the values are determined.

Example 3.5.1

A boiler has a ‘from and at’ rating of 2 000 kg/h and operates at 15 bar g. The feedwater temperature is 68°C.

The use of Equation 3.5.1 will determine a factor to produce the same result:

Note: These values are all from steam tables.

Using the information from Example 3.5.1 and the Equation 3.5.1 the evaporation factor can be calculated:

kW rating

Some manufacturers will give a boiler rating in kW. This is not an evaporation rate, and is subject to the same ‘from and at’ factor.

To establish the actual evaporation by mass, it is first necessary to know the temperature of the feedwater and the pressure of the steam produced, in order to establish how much energy is added to each kg of water. Equation 3.5.2 can then be used to calculate the steam output:

Example 3.5.2

A boiler is rated at 3 000 kW (kJ/s) and operates at 10 bar g with a feedwater temperature of 50°C. How much steam can be generated?

Where, from using the tables on the Spirax Sarco website:

Boiler hor​sepower (BoHP)

This unit tends to be used only in the USA and Australia. A boiler horsepower is not the commonly accepted 550 ft lbf/s and the generally accepted conversion factor of 746 Watts = 1 horsepower does not apply.

USA and Australia

In the USA and Australia the readily accepted definition of a boiler horsepower is the amount of energy required to evaporate 34.5 lb of water at 212°F atmospheric conditions.

Example 3.5.3

A boiler is rated at 500 BoHP, what is its steam output?

Important: This is essentially the same as a ‘from and at’ rating, so using feedwater at lower temperatures and steam at higher pressures will reduce the amount of steam generated.

In practice: A BoHP figure of 28 to 30 lb / h would be a more realistic maximum continuous rating, taking into account the steam pressure and average feedwater temperatures.

A more practical result would then be:

Consequently: If 17 250 lb/h of steam is required, a 500 BoHP boiler would be too small, and the user would need to specify a boiler with a rating of:

Your closest Spirax Sarco is